The e-spool flex 2.0 is the igus version of a cable drum without a slip ring. Cable diameters from 5mm to 15mm can be used. The cable is always safely routed through a feed-through to ensure that it is wound up correctly.
No additional copper components in the system (apart from cable copper)
Parts are reusable
Less raw material required thanks to the option of partial repair instead of complete replacement
Have your energy chain recycled at the end of its life cycle with the igus Chainge recycling program . Irrespective of the manufacturer. You will receive a voucher for: chainge recycling program
igus has been an investor in Mura Technology from the beginning and is helping advance chemical recycling. From plastic waste to crude oil in 20 minutes.
Installation instructions
The illustrated assembly aid enables you to assemble the e-spool flex 2.0 and e-spool flex mini quickly and professionally.
Note: Please consider VDE 0298 Part 5 (Current carrying capacity and conversion factors for wound cables) when selecting your cables and when using e-spool flex
NEW: e-spool flex accessories
Now with guide roller and brush attachment (optional)
Brush unit
Brush attachment for cleaning the cable before rolling it up.
Guide roller
Idler pulley for "around the corner" extension.
Documentation
Documentation cable drum e-spool flex
This documentation will provide you with all important information about e-spool flex - from technical data to hazard warnings to safety instructions.
This documentation will provide you with all important information about e-spool flex mini - from technical data to hazard warnings to safety instructions.
White paper: slip ring-free cable reel with screw guide
With a newly developed cable reel for control panels, robot users avoid "cable tangle" and tripping hazards in automated production. Since the new solution does not use slip rings, media, data and the power and signal supply of the emergency stop button can also be integrated into the system. Download the white paper to find out more.
Discover the structure of the e-spool flex in the video.
Cables or hoses are inserted into the e-spool in a spiral pattern
The e-spool flex in detail from the inside (from left): housing, worm guide, cables/hoses, winding housing
The e-spool flex in detail from the outside (from left): housing, worm guide, cables/hoses, winding housing
Detail: cable/hoses inserted in the worm guide
Extension lengths up to 15m possible
Possible uses for the e-spool flex 2.0
... on industrial robots
... in the car repair shop
... on platforms
... in harbours
... in the warehouse
Possible uses of the e-spool flex mini
... at the dentist's
... at charging stations for e-bikes
... in the office
Tested in the igus laboratory
For e-spool flex pull-out forces
In its test laboratory, the largest in the industry, igus compared the e-spool flex with a competing product. The test evaluated the two products' pull-out forces.
The results showed that the e-spool pull-out forces were about ten newtons, while those of the competing product were almost twice that.
In its test laboratory, the largest in the industry, igus compared the e-spool flex mini with a competing product. The test evaluated the two products' extension lengths.
The results showed that the e-spool flex mini extension length was about three metres, while that of the competing product was only half that.