#1, Survey No. 34,
Mandur-Devanahalli Road, Mandur Village, Bidarahalli Hobli,
Bangalore- 560049
The system works via a telescopic arm on the RTG, which can be extended and retracted. This has two advantages: Firstly, it enables automatic coupling and the energy chain, in which all media can be guided simultaneously, is pulled along by the RTG. This ensures the supply of energy and data. Secondly, horizontal and vertical unevenness and offsets in the travel can be compensated. The system is suitable for long travels - 500 metres and more are possible, depending on customer requirements in the container port. |