Handling system ”roboLoop“
The ”roboLoop“ system itself offers manyways to optimise the fabrication sequences.

Modern plastic energy chains® are the umbilical cord of the automation, machine and plant engineering industries. These energy chains® ensure the safe supply of energy, data, pulses and operating media and are always in motion. Energy chains® are suitable for multipurpose use in the crane and machine tool industries and in the robotics and clean room industries.
The ”roboLoop“ system itself offers manyways to optimise the fabrication sequences.
The rail & Tracking systems are used wherever fast camera movements are an important factor as, for example, at sport competitions, but also at many popular events such as concerts, stage shows, etc.
A plastic chain makes any kind of maintenance on the open sea obsolete; a conventional metal chain would not be adequate for the combination of technical, climatic and mechanical requirements.
Theproblem with previous data glove solutionswas that the sensors in the gloveswere subject to extreme loads and thatmovement signals were also producedunintentionally during sideways movements.
This telescope has been installed on theCanary Island of La Palma and registersthe gamma rays that strike the earth fromouter space.
A solution for media elevators previously unavailable in the market has now beenrealised with igus® E-Chain Systems®.
The door systems in this application guaranteethat the temperatures prescribed for the productand storage of perishable products, such asfood, are strictly observed.
The destination point for the energy and control is variable and can lie at a height of ten meters.
The used igus® products prove themselves till today and drastically reduce the maintenance input.
The previous travelling cables below the elevator cars were exposed to a steady air draft through an enforced ventilation for the smoke detector system and an undesirable sideward movement developed.
This application showed that a vertical stroke of more than one metre and a swivellingrange of 270° can be implemented in the limited installation space of the grinding headin a gear-grinding machine.
TheE-Chain® was installed on an injection moulding tool so thatno additional space is necessary in horizontal direction forthe unreeling movement.
In the case of this industrial robot, a rigid pipe between the 3rd and 6th axis wasreplaced by a multidimensional, flexible Triflex® R energy chain®.
This machine moves deeply through the earthand is used to drill tunnels using the excavationby mining technique.
This drill, the Vibrocorer VKG-6, is used in extremely demanding environments. a
For this application, aircraft engine parts arewelded together.
The rotary motion in both directions by up to 310° is also possible at high speeds of up to 20 meters per second.
Since most elevator malfunctions are the result of defective doors, an extremely reliable, space-saving solution became necessary here.
The ”Virtu“ large-format printer can be used to print almost anything: sheetmetal, foils, textiles, wood, glass, and, of course, also paper in widths up3.5 metres.
In the case of these robots, the hosepackage had to be replaced very fewweeks.
This newly developed stern thruster helps sailboats during difficult manoeuvres such as, for example, passages through locks;but because of its high performance, it can also be used as a main drive unit.
The marking system moves like a robot with several axles. In the process, the energy supply system should remain accessible and should be laid as compact as possible in the machine to prevent collisions with other machines.
Medical students and physicians can practise diverse vascular surgicalinterventions on this device.
A very high acceleration provided an enormouschallenge for the design engineers of this robot.
This newly developed gas-fired furnace only requires onethirdof the usual time to heat up rollers in the steel industry
This energy chain® in the palletising system of a dairy is subject toextreme load with more than 5,000 strokes a day.
This crane in a truck assembly plant is used to unload andtransport the individual vehicle chassis at the beginning of the assembly process.
To control andsupply the lying surface area, data and electrical cables, including hydraulic hoses, are run along the column.
Almost daily failures of this inclined hoist in the URBIS art centre in the Manchester citycentre have become a thing of the past with the deployment of the igus® E-Chain®.
This height-adjustable design speaker’sdesk is very flexible in its features.
The igus® E-Chain® E6 demonstrates its strengths inthe case of this cutting tool.
In this application in a painting robot, the ATEX properties of the energy supply system are of primary importance.
This workpiece storage location is designedfor automated shift operation. At the same time, the energy supply mustbe provided in all four axes of motion(three linear axes and one rotational axis).
The modules are made of a cable-preserving plastic with high frictional resistance.
For the handling of printed circuit boards, a six-axis robot is used in the case of this application instead of the usual linear systems.
To save installation space and toreduce forces and torques, an E-Chain® was wound around a gripper.
The special feature of thisapplication is the hot chips produced during the machining process, which do not stick tothe igus® E-Chain® and therefore extremely reduce the maintenance expenditure as a result.
The driven boring machine produces extremevibrations and heavy soiling duringthe work process.
The igus® E-Chain® B17 was just completely alienated from its intended purpose for this clever application.
In the case of this application, the worksafety was increased by integrating theenergy supply system into the body of thepallet changer.
Visible for approx. only one minute are these pictures, which are ”printed“ with UV lighton a light-sensitive screen.
Until recently, you could not purchase a solution anywhere in the world for this application.
With the perfectly fitting energy supplysystem for this crane system, the overalldimension for the installation was considerablyreduced.
This laser welding robot works extremely fast. Here, a very flexible and, above all, fail-safe energy supply system is required.
The used E-Chain® of the E2 mini family is suitable for all requirements and has already completed six years without failure.
In the case of these gate drive units, different products from all the igus® divisions are used.
After its completion, this giant telescope in Arizona(USA) will look deep into our universe; the two mainmirrors each have diameter of 8.4 metres.
In the case of this adhesive resin system, a lifting platform moves upwardto a height three or four times a day to empty barrels with a volume ofapprox. 200 litres.
Under the difficult ambient conditionsexisting outdoors, the presentsystem with a motor-powered cabledrum proved to be not resistantenough.
Previously, several individual hoses had to be fastened in the energy supplysystem to prevent them from squeezing each other.
Incidental grinding residues and the used oil cannot influence the energy supply systems.
One igus® E-Chain® of the E6 family accelerates the work sequences in the case of this application for wafer handling in the chip production industry.
Measuring and regulating system in the area of blown film extrusion
The previously used energy supply system as a rule wore out after nine months; the cables were destroyed by hot chips, which led to production failures.
Prior to the use of the E-Chain®, the cables were fastened with cable ties. That frequently led to entangled cables and the corkscrew effect, which lets the cables become susceptible to core ruptures.
During the removal of a nuclear power plant, 14 metre-high steel tanks are milled into small metal chips. At the same time, a milling cutter, which is used as a dismantling tool, must be inserted precisely into the tank from above.
These applications are dependent on a compact energy supply system, for which the accumulating wood chips do not matter.
As large heavy quantities are to be weighed, the existing energy supply system had to contend with high wear.
Monitoring of the growth of plants in a conservatory.
In this paint-spraying machine, sensors aremoved over minimum space.
For some applications that require high electric power, conventional copper cables aretoo heavy.
igus® contact+91-80-39127800Send e-mail to igus®
myigusProduct finderOnline catalogApplication examplesNews 20103D-CADProduct comparisonService life calculationShelving configuratorSpecification of
E-Chains®3D CAD configurator for E-Chains® with circular motionTwisterChain®
3D CAD configurator for spiral E-Chains®Email the product expertDesign informationAssembly InstructionsInquiry/orderQuickSpecPart No. searchCatalogs/samplesDownload