Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

chainflex® flexible cable applications

igus® developed chainflex® continuous flex cables in the 1980s after an increase in the demands of automation technology meant guided cables often failed, despite the cable carrier continuing to function perfectly. In some cases, failures caused by "corkscrews" and core ruptures brought entire production lines to a halt and resulted in high costs. In order to find a solution to this unsatisfactory situation for its customers, igus® decided to take the initiative and create unique cable-design principles to help prevent machine downtimes in factories throughout the world.

Search Customer Applications


Filter applications by industry, applications, etc.


Indoor and outdoor cranes

Indoor cranes work in very high temperatures, while the outdoor cranes withstand severe coastal weather.

No cable breakage

chainflex® continuous-flex cables eliminated problems with cable breakage.

Service life clearly enhanced

Since switching to chainflex® continuous-flex CF9 and CF10 control cables, service life has dramatically increased.

LED screen at Victory Plaza in Dallas

Temperature-resistant cables and cable carriers mean the larger-than-life size LED screen at Victory Plaza in Dallas functions despite heat, sun, rain and snow.

flizz® sewage treatment plant

flizz® cable carrier system including and chainflex® cables instead of a cable drum. Smooth operation at this sewage treatment plant since 2000.

Subway train door

chainflex® CF98 control cables used in the pneumatically operated passenger doors on subway trains.

Stacking unit for phosphorous screens

chainflex® CF98 used in stacking unit for phosphorous screens

Roller cable carriers for a composting plant

These roller cable carriers and chainflex® cables operate despite extreme conditions in this compost plant

Furniture factory

chainflex® control cables have to be flexible enough to cope with 14-hour work days on this leather-cutting machine.

Woodworking machining center

Pre-assembled readychain® cable carriers for woodworking machinery.

Turning-and-grinding machine

This machining center uses seven cable carrier systems, two of which are fully pre-assembled readychains®.

Amusement park ride

Ship-to-shore cranes cable carrier

Cable carriers and cables on marine applications

Micro flizz® in cold storage rooms

Micro flizz®: Quick and neat cable carrier system for high-speed roller door, including chainflex® cables

Cable Carrier for Brickworks

Application of cable carriers and continuous-flex cables in tile factory

readychain® pre-assembled cable carrier systems

Pre-harnessed cable carriers and cables for automated machinery

Servo motor feedback cables for machining centers

readychain® pre-harnessed cable carriers with chainflex® cables: from special design to standard model

Cable carrier -machining center

readychain® cable carrier systems using in a machining center

Woodworking machine tool

This company decided to use pre-assembled readychain® cable carriers in a new machine tool series.

Container Crane: Malaysia

Close to 1,500 ft (441 m) travel and loads up to 2.5 tons on a container crane in Malaysia.

Ship loader

Wind and weather proof, energy chain cable carrier and chainflex® cables on a ship loader at the Baltic Sea port of Wismar.

OpenHydro tidal turbine

This OpenHydro tidal turbine generates electrical power through the inflow and outflow of water.

Crash simulation robot

Very high accelerations proved an enormous challenge for the design engineers of this robot.

Automatic gates

Cable carriers and continuous-flex cables for belt-driven automatic gates

Underwater boring machine

This drill is used in extremely demanding offshore environments and uses continuous-flex cables from igus®

Dismantling tool for nuclear power plant decommissioning

Dismantling tool for nuclear power plant decommissioning

Car wash cable carrier

Touch-free car wash uses System E4/4 cable carriers and chainflex® CF140 US cables.

Application Assistance

For further questions or product information, please contact:

Photo
Timothy Marran

chainflex® Product Manager

Email

Customer Service:

Monday to Friday from 8 am - 8 pm

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302