Rolling bearing grease? No, thank you!


Technical data

  • What was needed? Quickly available and cost-saving ball bearings
  • Requirements: Low rolling friction, freedom from lubricants, weight reduction
  • Material: xirodu B180
  • Industry: Bonding technology
  • Success for the customer: The polymer ball bearings from igus are half the price of the conventional solutions previously used than metal.

Go to tesa scribos®:The company is an expert in the field of pioneering adhesive solutions such as counterfeit and theft protection in the form of adhesive seals. The goal of tesa scribos® was to find cost-effective and maintenance-free ball bearings that are used in guide rollers. There the function of a deflection in the pressure roller before an intermediate drive should be performed.
 
The pressure roller is set with a defined compressive strength on the drive roller. The combination of guide roller and intermediate drive not only serves to drive the product, but also creates web tension in the material, whereby different wrap angles can be set on the intermediate drive by means of the variable position of the guide roller. The different coatings of the rollers serve to protect the material as well as to improve material handling.
Coated guide roller with xiros® B180 deep groove ball bearing

Problem

In the past, metallic ball bearings were used, which could only achieve low rolling friction with appropriate lubrication. The tesa scribos® was looking for a ball bearing solution that offered an optimised savings potential, not only in terms of maintenance and weight, but also in price.

Solution

The now used xiros plastic ball bearings from igus® are half the price and available faster than the previously used ball bearings. The user also benefits from the lightweight, the low friction and the freedom from lubrication of the plastic ball bearings.

In search of a complete solution?

xiros guide roller: online shop


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH