Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

e-cord micro protects the smallest hoses01-09-2014

Modular system from igus to guide and protect very small hoses and cables

Moving small scale capillary tubes reliably and safely often poses major problems for design engineers, especially in the medical industry. igus has now developed the e-cord micro system to address this. The modular system of straight, curved and mounting parts, means that even the smallest tubes can be fitted into moving equipment with confidence.

Medical machines often contain dosing and pipetting functions which require the constant movement of capillary tubes, which are only a millimetre or so in diameter. In these applications the fragile capillary tubes are often squeezed into a small bend radius which can cause damage to the tubes or blockages in the flow through them. igus has designed the e-cord micro to help in these cases. The system ensures the hoses do not fall within a pre-defined minimum bend radius of 45mm, and are also given some physical protection. The modular nature of the system and the elasticity of the material allows machine designers lots of flexibility when designing moving capillary tubes into the smallest of spaces.

Modular Design
igus assembles the e-cord micro to order, ensuring a perfect match to the required motion and space of the machine. In this way, different movement directions and travel path lengths can be implemented easily and flexibly. The concept for the e-cord micro, like many other igus products, was driven by customer requirements for a novel solution to their specific challenges. By producing a flexible solution, many other applications in different industries can be realised too.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH